Technical FAQs

Ask a Question

Any Acti 9 devices equipped with a Ti24 connector can be connected directly to a PLC without Smartlink.

If the PLC is compliant with IEC 61XXX, then Acti 9 devices equipped with a Ti24 connector can be connected directly to a PLC without Smartlink.
Was this helpful?
What can we do to improve the information ?