Technical FAQs

Ask a Question

At what temperature value temperature controlled switch is operated in protected type braking resistors designed for Altivar 312 drives

Protected braking resistors VW3A701 to VW3A705 integrated with temperature controlled switch that becomes operational at 120’C temperature
Was this helpful?
What can we do to improve the information ?