Technical FAQs

Ask a Question

What are the logic addresses for display parameters - O01 to O50 of controller inside that can be displayed on graphic display of altivar 61 / 71

Logic addresses of display parameters O01 to O50 starts from 6401 and is up to 6450 respectively.

Was this helpful?
What can we do to improve the information ?