Technical FAQs

Ask a Question

Which Modbus functions are used for reading/writing multiple data on IO scanning in Modicon Quantum range.

In Modicon Quantum range, I/O scanning works with following Modbus function codes:
 
  1. FC3 for Reading Multiple 4X registers.
  2. FC16 for Writing Multiple 4X registers.
  3. If both the read and write are filled out then FC23 for Read/Write Multiple 4X registers is used.
Was this helpful?
What can we do to improve the information ?