Technical FAQs

Ask a Question

Can we use Proworx32 140CPU53414A / B cpu on Unity platform

The cpu's 140 CPU 534 14 A/ B  can be upgraded to be compatible with the Unity Pro software without any hardware modifi cation. This process of migration is achieved by updating the CPU operating system with Unity OS. This update is performed with the aid of the OS-Loader tool included with Unity Pro. The migration of 140 CPU 534 14B processor requires the version of Unity Pro > 3.0

Was this helpful?
What can we do to improve the information ?