Technical FAQs

Ask a Question

What are the considerations need to be take care for a web client license point counts in a Vijeo citect project.

If you are using web clients in your project then the number of license point counts should be same as on IO Server license key as the web client seek for its web client license strictly limited on requesting the license from the IOServer and you can not use web client with a local license (static) instead of floating license.
Was this helpful?
What can we do to improve the information ?