Technical FAQs

Ask a Question

Can we use the BACnet driver with Vijeo Citect 7.30,If yes then do we need to purchase separate license for this driver in Vijeo Citect SCADA.

Vijeo Citect SCADA supports the BACnet protocols. You have to go for " +  Facilities pack " for including the BACnet driver in Vijeo Citect. The BACNET driver is designed to communicate with BACnet networks and devices using the BACnet/IP transport option. This "+Facilities Pack" is licensed and you have to purchase separate license for that pack .You can download the latest driver version of BACNET from:
http://www.citect.schneider-electric.com  >>  Struxware SCADA Expert Vijeo Citect   >>   Driver Web .



 
Was this helpful?
What can we do to improve the information ?