Technical FAQs

Ask a Question

Can i use Quantum QERIO HotStandby architecture without using CRP module

The minimum configuration required for QERIO Hot Standby based architecture is two identical plc racks with :-
1. Power Supply
2. CPU controller module
3. CRP module

Was this helpful?
What can we do to improve the information ?