Technical FAQs

Ask a Question

Is it possible to connect NeoBreak RCCB 4P, 220 ... 240 V AC in three-phase without neutral application.

Yes, it possible to connect NeoBreak RCCB 4P, 220 ... 240 V AC in three-phase without neutral application.

Please refer the below connection diagram


Was this helpful?
What can we do to improve the information ?