Technical FAQs

Ask a Question

Is there any external PTC temperature sensor available for ClimaSys CC Thermostat and Hygrostat range of products.

The NSYCCAST is the product reference of PTC external temperature sensor which is same for both Thermostat and Hygrostat and is required for remote reading.
  • Length : 3 metres
  • Several types of fixing ( on DIN rail, on Spacial SF profile, on VDI cross-rail, on mounting plate )
  • Sensor operation or reading range -30°C to 80°C .
  • Protection rating : IP67
Please refer the below attachments for the instruction sheet of NSYCCAST.
Was this helpful?
What can we do to improve the information ?