Technical FAQs

Ask a Question

What is the Relative Humidity for EasyPact CVS circuit breaker as per the damp heat test of IEC 60068-2-30 standard.

The Relative Humidity of EasyPact CVS circuit Breaker is 95 % at 55°C as per the damp heat test of  IEC 60068-2-30 standard.


Was this helpful?
What can we do to improve the information ?