Technical FAQs

Ask a Question

Can I launch other applications from Unity Pro

Yes, this can be done by choosing 'Customize' under <Tools>. Go to the 'Tools' tab and hit the 'Add' button and type in the name of the application in the 'Menu Text:'

Under 'Command' type in the path to the application. In the case of the Microsoft Event Viewer, this will be :
Hit <OK>.
From the menu line, expand <Tools> and 'Event Viewer' will appear as a choice at the bottom of the drop down box. Clicking on Event Viewer will bring up the Microsoft Event Viewer which can be used to view the Audit Trail set up in the Unity Security Editor.


Was this helpful?
What can we do to improve the information ?