Technical FAQs

Ask a Question

Can I use the Device Control Block as a means to modify entries in the IO Scanner Table

You cannot use the Device Control Block as a means to modify the IO Scanner Table. The purpose of the Device Control Block is to allow the user to turn an IO Scanner Table entry on or off while the application is running. Adding new table entries or deleting existing entries must be accomplished offline because it's considered to be a configuration change and will require a full download.
Was this helpful?
What can we do to improve the information ?