Technical FAQs

Ask a Question

Does the M340 product line meet the "Finger Safe" or IEC 60529 specification

IEC 60529 is the standard for Ingress Protection. The M340 product line is IP20 rated which is considered "Finger Safe".
Was this helpful?
What can we do to improve the information ?