Technical FAQs

Ask a Question

How do you write a value to all of the words in a table using Unity Pro

You use the " MOVE_INT_ARINT " command in Unity Pro software.

A example of the syntax to write a value of 1 to all the %MW words in the table with the Operate Block is as follows:
The above syntax writes a value of 1 to Memory Words 100 to 199 ( %MW100 to %MW199)
There is also a EFB of the same name (" MOVE_INT_ARINT ") and does the same function.
Below both ways are displayed.

Was this helpful?
What can we do to improve the information ?