Technical FAQs

Ask a Question

What are the dimensions of the INS400 single handle transfer switch 31150?

205mm x 395mm x 155mm (H x W x D) excluding the handle.
Overall depth with standard handle is 213mm.
See attached.
Was this helpful?
What can we do to improve the information ?