Technical FAQs

Ask a Question

Ethernet communication card - VW3A3320 for Altivar 61 / Altivar 71 drives supports which protocols

 

Ethernet communication card - VW3A3320 supports protocols (1) Ethernet I/P and (2) Modbus TCP/IP. When this card is inserted in ATV61/ ATV71 drives,
user will have option to choose one protocols

With EtH [Ethernet]  menu, parameter EtHn [ Ethernet protocol] is there that decides selection between Ethernet I/P and Modbus TCP/IP protocol. 

Was this helpful?
What can we do to improve the information ?