Technical FAQs

Ask a Question

What is the power factor of Altistart 48 Soft Starter.

The power factor depends on the power factor of motor. 
The aim of the Soft Starter is to increase the motor speed at the nominal speed and at the end of the starting, it bypasses via contactor. So the power factor depends on the cos phi of motor.
Was this helpful?
What can we do to improve the information ?