Technical FAQs

Ask a Question

Which ION meter models and firmware supporting IEC61850 communication protocol

Your ION meter must have Ethernet communications and be a model that supports IEC 61850. New meters can be purchased with IEC 61850 or IEC 61850 firmware can be loaded onto an existing meter.
Refer below meter models and meter firmware support IEC 61850:

Meter Model:

Meter Firmware:
Was this helpful?
What can we do to improve the information ?