Technical FAQs

Ask a Question

What is overview principle of IEC 61850 communication protocol

IEC 61850 is an Ethernet-based protocol designed for electrical substations. It is a standardized method of communications, developed to support integrated systems composed of multi-vendor self-describing IEDs (Intelligent Electronic Device) that are networked together to perform monitoring, metering, real-time protection and control. 
Was this helpful?
What can we do to improve the information ?