Technical FAQs

Ask a Question

When I click on an empty EFB ANY pin in logic and select the ellipsis to add a variable, only IODDT variables are displayed, no elementary variables

Make sure that 'inside structure' is not checked. If it is, ONLY structured variables will be displayed.
Was this helpful?
What can we do to improve the information ?