Technical FAQs

Ask a Question

Why I am unable to connect M580 CPU using Unity Loader

Unity Loader will not connect if it cannot establish connection to ftp. A M340 CPU has inbuilt feature of Cyber Security, due to this enhancement by default the CPU's ftp service is disabled. So for getting connected Enable ftp on your CPU. To do so, load an application into the CPU that has FTP enabled.

Was this helpful?
What can we do to improve the information ?