Technical FAQs

Ask a Question

What is meaning of "bridge mode" in 140NOM2xx00 module

The 140 NOM 2xx 00 are modbus plus option modules which has modbus plus as well as a modbus connector on them. A bridge mode capability in the module permits a panel device connected to modbus port to access nodes on the Modbus Plus network or to access the local PLC directly without having to go out onto the network.
Was this helpful?
What can we do to improve the information ?