Technical FAQs

Ask a Question

How to modify the number of COM ports used by the TSXPCX3030 programming cable in Windows2000 and WindowsXP.

The number of COM ports used by the TSXPCX3030 programming cable can be modified in Windows2000 and WindowsXP by following the below mentioned steps:
 

  1. Go to the Control Panel
  2. Double-click on the System icon
  3. Select the [Hardware] tab
  4. Click on [Device Manager]
  5. Expand the Ports (COM & LPT) branch
  6. Double-click on [Serial port, USB multifunction cable (COMx)]
  7. Select the [Port Parameters] tab
  8. Click on the [Advanced] button
  9. Modify the number of the COM port
  10. Confirm
Was this helpful?
What can we do to improve the information ?