Technical FAQs

Ask a Question

How to establish communication between the programming computer loaded with PL7-Pro and TSX37 or TSX Nano slave via Uni-Telway Bus.

To communicate between PL7-Pro loaded in the programming computer and TSX37 master via Uni-Telway bus, the 'SYS' (system) address must be entered in PL7 Pro.

A sufficient number of addresses must be configured in the master and addresses 1, 2 and 3 must be reserved for PL7 Pro.

To communicate between PL7-07 and TSX Nano slave via Uni-Telway bus, address'x' must be entered in PL7-07, where 'x' is the TSX Nano slave address.
Was this helpful?
What can we do to improve the information ?