Technical FAQs

Ask a Question

What is the MTBF (Mean Time Between Failures) value of Lexium 23 range of servo drives

MTBF values for Lexium 23 range of servo drives are as below.

Lexium 23A/D range:

LXM23xU01/02/04M3 : 4382,61hours
LXM23xU07/10/15M3 : 4328,26hours
LXM23xU20/30M3 : 4315,55hours
LXM23xU45M3 : 4235,21hours
LXM23xU55M3 : 3713,10hours
LXM23xU75M3 : 3709,79hours
 
Lexium 23C/M range:
 LXM23CU01M3 :7416,92hours
LXM23CU02M3 :7416,92 hours
LXM23CU04M3 : 7436,47 hours
LXM23CU07M3 : 7371,38 hours
LXM23CU10M3 : 7321,18 hours
LXM23CU15M3 : 7321,18 hours
LXM23CU20/30M3 : 7028,71 hours
Was this helpful?
What can we do to improve the information ?