Technical FAQs

Ask a Question

On which protocol data are exchanged with NVL (Network variable List) functionality in SoMachine range controllers

In SoMachine range of controllers, data are exchanged through UDP ( User datagram protocol) on IP (Internet protocol). It is UDP/IP protocol.

Was this helpful?
What can we do to improve the information ?