Technical FAQs

Ask a Question

What is the wireless and battery less push buttons XB5RFA02 and XB5RMA04 Kit constitution and what is the difference between these them

1.
Kit constitution of XB5RFA02 is as below

ZBRRA - configurable Receiver
ZBRT1 - Transmitter
ZB5AZ009 - Fixing collar in plastic
ZB5RZA0 - Flush push type spring return push button head in plastic (Without CAP)
ZBA79 - Set of 10 different colored caps with different markings. White, black, green, red, yellow, blue,white I on green background, black I on white background, white O on red background, white O on black background. (1 cap to be selected and fitted)

2.
Kit constitution of XB5RMA04 is as below

ZBRRA - configurable Receiver
ZBRT1 - Transmitter
ZB5AZ009 - Fixing collar in plastic
ZB5RZA0 - Flush push type spring return push button head in plastic (Without CAP)
ZBA79 - Set of 10 different colored caps with different markings. White, black, green, red, yellow, blue,white I on green background, black I on white background, white O on red background, white O on black background. (1 cap to be selected and fitted)

Difference between XB5RFA02 and XB5RMA04 is that in XB5RMA04 Wireless and batteryless pushbutton + Ø 22 mm/0.866 in. plastic head mounted in a handy box. Such box type mounting is not there for XB5RFA02.
Was this helpful?
What can we do to improve the information ?