Technical FAQs

Ask a Question

What are the CANopen communication interface options for Altivar 32

The Altivar 32 can be connected to a CANopen network by several ways:

• The first solution is to use a CANopen communication adapter that can be locked in the option slot of the drive 

  VW3 A3 608 - Dual RJ45 Module
  VW3 A3 618- CANOpen connection with SUBD9
  VW3 A3 628 - Open style 5 pole connector

• The second solution is to use the communication base port in the front of the drive (Integrated port)

The CANopen base port will become inactive when an option card is inserted.
Was this helpful?
What can we do to improve the information ?