Technical FAQs

Ask a Question

What type of isolation is there in BMXAMI0810 analog input module.

The BMXAMI810 Modules have optical isolation and the value of isolation is as below:-

Between channels    +/-300 VDC
Between channels and bus    1400 VDC
Between channels and ground    1400 VDC

Was this helpful?
What can we do to improve the information ?