Technical FAQs

Ask a Question

Can the serial link module BMXNOM0200 used in a Quantum Ethernet X80 drop.

When this Serial Link module BMXNOM is used in a Quantum Ethernet I/O X80 drop, it must have:
Product software = 04
 Firmware version ≥ 1.4

This information is visible on the label on the side of the module.

NOTE: This module is referred to as BMX NOM 0200.3 in Unity Pro configuration screens and in the Unity Pro software documentation.
Was this helpful?
What can we do to improve the information ?