Technical FAQs

Ask a Question

What is the maximum numbers of slave devices handled on CANOpen network with M258 CANopen master

M258 supports maximum 63 numbers of slave devices on CANopen with limitations of maximum 126 RPDO (Receive PDOS) and 126 TPDO (Transmit PDOS)
Was this helpful?
What can we do to improve the information ?