Technical FAQs

Ask a Question

What is the maximum numbers of slave devices handled on CANOpen network with LMC058 Motion controller

LMC058 motion controller integrated with 2 CAN ports. CAN0 and CAN1
LMC058 can handle 2 independent CANOpen networks at the same time (one with CAN0 port and the other with CAN1 port) Each port (CAN0 or CAN1) can handle Maximum 63 numbers of slave devices with limitations of maximum 126 RPDO (Receive PDOs) and 126 TPDO (Transmit PDOS)
Was this helpful?
What can we do to improve the information ?