Technical FAQs

Ask a Question

Does Maximum counting frequency of HSC (High speed counter) of SoMachine depend on any settings. If it depends what is it

Yes, maximum counting frequency of HSC of SoMachine depends on the set filter value of counting inputs
For one shot and Modulo loop mode of HSC Simple type, One shot mode of HSC Main type, Event counting mode of HSC Main type and Frequency meter mode of HSC Main type counter Pulse A is the counting pulse.
For this below is the relationship of Maximum counting frequency with Pulse A filter value
  • Maximum counter frequency is 100 KHZ if filter for counting input is set to 0.004 ms (default)
  • Counter frequency is 1 KHZ if filter for counting input is set to 0.4 ms
  • Counter frequency is 400 HZ if filter for counting input is set to 1.2 ms
  • Counter frequency is 100 HZ if filter for counting input is set to 4 ms
 
For Modulo loop mode of HSC Main type and Free large mode of HSC Main type counter pulses A and B are the counting pulses
For this below is the relationship of Maximum counting frequency with Pulse A and Pulse B filter value
  • Maximum counter frequency is 100 KHZ if filter for counting input is set to 0.004 ms (default)
  • Counter frequency is 1 KHZ if filter for counting input is set to 0.4 ms
  • Counter frequency is 400 HZ if filter for counting input is set to 1.2 ms
  • Counter frequency is 100 HZ if filter for counting input is set to 4 ms
Was this helpful?
What can we do to improve the information ?