Technical FAQs

Ask a Question

What are the correct ways for assigning drive parameters to IO scanners of Ethernet card VW3A3310 (Modbus TCP/IP card Ethernet card) or VW3A3310d (Modbus TCP/IP Ethernet daisy chain card) or VW3A3320

Drive parameters can be configured to IO scanners of Ethernet card only through either PC-software workshop (SoMoveLite) or through Ethernet card – standard Web server.
Drive parameters assigned to IO scanner through integrated display terminal or Graphic display terminal of drive will not be taken into the effect and hence those particular drive parameters will not be exchanged to IO scanner of Master PLC or controller
Was this helpful?
What can we do to improve the information ?