Technical FAQs

Ask a Question

What are the different scenarios of Ready LED in Compact NSX?

The different scenarios of Ready LED in Compact NSX is as shown in the attached. 
 
Note: Ensure that the trip unit is correctly supplied i.e. primary current above indicated value (example: >30A, depends on the rating) or supplied from a 24V external power supply or supplied with the pocket battery.
Was this helpful?
What can we do to improve the information ?