Technical FAQs

Ask a Question

What is the part reference number for the BacNet on Ethernet driver that supports Power Logic Scada (PLS/PSE) ver 7.30.

To use BacNet driver with Power SCADA Expert V 7.30 (PLS/PSE), Use the "+Facilities" driver pack which includes the BacNet & Konnex driver. Purchase of separate license is required for this " + Facilities" driver pack. So need to order this part reference PSA305501 as the driver reference pack for this "+Facilities" driver pack and need to add this on your PLS/PSE license key.
Was this helpful?
What can we do to improve the information ?