Technical FAQs

Ask a Question

Does the MPPT60-150 have a GFP?

MPPT60-150 Ground Fault Protection Specifications 
 The MPPT60-150 unit has an Internal Ground Fault Protection, the specifications for this can found bellow:

This feature can be disable if the customer has an external GFP, the steps to do so are found on the Operations Manual attached on page 2-9
Was this helpful?
What can we do to improve the information ?