Technical FAQs

Ask a Question

What is the voltage tolerance level at nominal voltage for the electrical auxiliaries used in Low Voltage Circuit Breakers

The voltage tolerance level for the electrical auxiliaries (example: undervoltage release(Mn), shunt coil(Mx)) used in Low Voltage Circuit Breakers is defined as per the IEC 60947-2 standard.
The tolerance level defined by IEC60947-2 is 0.85% for minimum nominal voltage (Un) and 1.1% for maximum nominal voltage (Un).
Example: For Un = 230/240V, Minimum tolerance Level is (0.85% of 230V AC) = 195.5V, Maximum tolerance Level is (1.1% of 240V AC) = 264V.
Was this helpful?
What can we do to improve the information ?