Technical FAQs

Ask a Question

What is the thickness of the Steel sheet metal of Blokset Panel.

The Steel sheet metal thickness used in Blokset Panel is as per the below table:

Blokset Steel sheet metal thickness

Housing Thickness mm
Door 2.00mm
Rear panels 2.00mm
Side panels 2.00mm
Roof/Top 2.00mm
Frame 2.00mm
Was this helpful?
What can we do to improve the information ?