Technical FAQs

Ask a Question

What are the Contact Resistance values for the SF1 Circuit Breaker.

The contact resistance values for the SF1 Circuit Breaker are tabulated below :

 

SF1

17.5 kV

24 kV

36 kV

Type 1

Type 2

Type 1

Type 2

Type 1

Type 2

Contact Resistance

current supplied : I = 100 A

< 70 µΩ

< 35 µΩ

< 70 µΩ

< 35 µΩ

< 75 µΩ

< 40 µΩ

Was this helpful?
What can we do to improve the information ?