Technical FAQs

Ask a Question

What is the state of the ATS48 Fault relay for various conditions?

Issue:
What is the state of the ATS48  “Fault” relay contact for the following conditions?

Product Line:
Altistart ATS48

Environment:
All models

Cause:
None

Resolution:
Relay R1 functions as a fault relay on terminals R1A-R1C when Menu IO, parameter r1 = r1F.
It is a normally open contact.

Conditions:
Control power not applied to CL1-CL2,  contact is OPEN
Control power applied and no fault,  contact is CLOSED
ATS48  detects a fault,  contact is OPEN

Note special case where Automatic Restart is active, Menu PrO, parameter ArS = ON.  When an Auto-Reset condition is detected, the R1 contact will remain CLOSED until all restart attempts are completed.  If the fault remains after the last attempt, then the R1 contact will OPEN.
Was this helpful?
What can we do to improve the information ?