Technical FAQs

Ask a Question

Is there a 'ready to close' PF contact available in Evolis 24 KV Circuit Breaker.

The 'ready to close' PF contact is available only for Evolis 17.5 kV with the Masterpact operating mechanism.
For the Evolis 24kV and SF or LF circuit breakers which use RI operating mechanism there are contacts for 'ready to close' but have a different nomenclature which is 'end of charging signalization', M3 Contact.
Refer the highlighted portion in the attached drawing.
Was this helpful?
What can we do to improve the information ?