Technical FAQs

Ask a Question

How to read the Real Energy value from PM 210.

The Real Energy consumption measured by PM210 is stored in two words, register addresses 4000 and 4001. It is a long analog type variable (long word).
 
The range of this register is in hexadecimal format is and between 0 and 0xFFFFFFFF. However, the register can hold a value up to 32767. If the measured energy value is larger, to prevent register data overflow, scale factor is used. This factor converts the register value within the range -32767 up to +32767. The scale factor is deposited in a single word register at address 4108.
 
Now to find out the Real Energy consumption measured value in PM210, follow the below steps :
  1. Read the first word (4000) in hexadecimal format. Example 0000;
  2. Read second word (4001) in hexadecimal format. Example 1ADF;
  3. Combine the registers value as 0001ADF and convert them into decimal format. 00006879
  4. Read the scale factor register value 4108. Example -2. This is a power of 10 and this means 0.01.
  5. Multiply 00006870x0.01 and the result is 68.7 kWh the Real Energy Consumption.
Was this helpful?
What can we do to improve the information ?