Technical FAQs

Ask a Question

Can the same mechanical interlock for LC1FL44 contactor be used for mechanical interlock of the new equivalent LC1F6304 contactor.

Yes, the same mechanical interlock LA9FL970 can be used for both the old LC1FL44 as well as for new equivalent LC1F6304 contactors. This is a horizontally mounted mechanical interlock.
For the new LC1F6304 contactor a vertically mounted mechanical interlock LA9FL4L is also available.
Was this helpful?
What can we do to improve the information ?