Technical FAQs

Ask a Question

What are the safety clearance dimensions for a LC1B range contactor switching with the DC voltage.

The safety clearance distances are as per the below table. These values are given for AC voltage; however these values are same as in case of DC voltage.

Note: With DC application the safety clearance in front of contactor will be 100mm (X1) and up to the arc chamber will be 150mm (X2) because the voltage per pole is limited to 440VDC.
Was this helpful?
What can we do to improve the information ?