Technical FAQs

Ask a Question

What is the part number of the Harmony Padlockable Flaps?

It is ZB4BZ6x, to which the number corresponding to the colour must be added: 2 = Black 4 = Red 5 = Yellow 6 = Blue
Was this helpful?
What can we do to improve the information ?