Technical FAQs

Ask a Question

Is the installation of 31097 locking kit same as the 31088 in Interpact source changeover system.

Yes, the installation of the 31097 & 31088 locking kits is the same, as all key locks have been designed to achieve locking in the OFF position.

Refer the attached Installtion guide for the key lock installation with 31097 kit on Interpact source changeover system INS 100A-630A.

Was this helpful?
What can we do to improve the information ?