Technical FAQs

Ask a Question

How many measurements can be configured to record in Data Log in PowerLogic PM5500 series meter.

Up to 14 selectable parameters with configurable interval and duration (e.g. 6 parameters for 90 days at 15 minutes interval).
The meter is shipped from the factory with data logging enabled for selected values. 
Typically, delivered energy (kWh, kVARh and kVAh) is logged by default, but you can configure the meter to record other measurements.
Was this helpful?
What can we do to improve the information ?