Technical FAQs

Ask a Question

How can we retrieve the logged data stored in PM 5300 & PM 5500 series via. ION Setup meter configuration utility.

>> Data log export using ION Setup; 
1. Start ION Setup and open your meter in data screens mode (View > Data Screens). See the ION Setup Help for instructions. 
2. Double-click Data Log #1 to retrieve the records. 
3. Once the records have finished uploading, right-click anywhere on the viewer and select Export CSV from the popup menu to export the entire log. 
NOTE: To export only selected records in the log, click the first record you want to export, hold down the SHIFT key and click the last record you want to export, then 
select Export CSV from the popup menu. 
4. Navigate to the folder where you want to save the data log file, then click Save. 

Was this helpful?
What can we do to improve the information ?